This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54361-Q1: Searching TI solution

Part Number: TPS54361-Q1

Hi Team,

There is a good new that we could DIN TI product!

Please help suggest products that meet the following specificationsTHX

Spec:

DC-DC
Synchronize
Jeter for good EMI
Can 4V~18V or ~ to 36V input
Can 0.9V output
Output 2A~3A
Frequency 2~2.2MHz
Automotive