I am using TPS63000DRCR
I have set it to output of 5V
When I provide less than 2V at its input and enable it, it goes short and absorbs around 1A of current. There is no load connected,
1. What is the inrush current?
2. What should be the behavior if I set a low limit of current on the lab supply? for example 300mA?