Part Number: TLV810SEVM-019
Hi,
I´m looking for a voltage detector able to detect cell low voltage conditions in each cell of a 12s battery pack. It would be placed on each line of the cell balance lines together with a P channel Mosfet, so it protects that cell from undesired undervoltage condition. Are there battery specific components with push-pull, active-high outputs? Are there other dedicated solutions for this kind of protection?
These protections would be placed between the BMS and the lipo pack, for cells protection in case of BMS failure.
I found TLV810S as a possible component, but this is not battery applications oriented. Are there other better (or more specific) components/solutions, or it would be a correct solution?
Thanks in advance.