This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54550: pull-up resistor to SSENA pin

Part Number: TPS54550

Hi Team, 

TPS54550's datasheet says "Do not use external pull-up resistors".  

But now customer is connecting another IC to SSENA pin and using pull-up resistor. 

Sometimes SSENA will be "L" which cause TPS54550's stops work. 

Maybe this phenomenon is caused by abnormal of IC connected to SSENA pin, 

but is there any possibility that this phenomenon is caused by the pull-up resistor? 

If yes, could you explain why this happens?

Thanks.

Regards,

Jo

  • Hi Jo,

    For your mentioned SSENA "L", I suspect that's pulled down by the another IC. For the pull-up resistors, if the voltage of another IC pin becomes 0, then it could be seen as a pull-down resistor. As you can see in datasheet, the internal current source is just 5uA, so if the external resistor value is not very large, the voltage 5uA*R cannot reach 0.5V.

    From my side, I would recommend customer to just follow our datasheet and not use external pull-up resistor. We can only guarantee the performance if the application follows our datasheet's recommendation.

    If customer wants to further check the root cause of this issue, I think the easy way is just to unpop the pull up resistor and see if the issue can be duplicated.

    Thanks,

    Andrew

  • Hi Andrew, 

    Thank you. 

    >For the pull-up resistors, if the voltage of another IC pin becomes 0, then it could be seen as a pull-down resistor. As you can see in datasheet, the internal current source is just 5uA, so if the external resistor value is not very large, the voltage 5uA*R cannot reach 0.5V.

    I couldn't get it well how can pull- up resistor becomes a pull-down resistor when the voltage of another IC pin becomes 0. 

    Could you help draw a picture to explain it? 

    For example, if 5V is connected to pull-up resistor, I think when the voltage of another IC pin becomes 0, 5V will applied to the pull-up resistor. So I think SSENA pin will just become 0V. 

    Thanks.

    Regards,

    Jo