Hi,
Are there two types of 1-pin markings for this product?
I don't know which one is correct, or if both are correct.
A type

B type
Thanks,
Masumi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are there two types of 1-pin markings for this product?
I don't know which one is correct, or if both are correct.
A type

B type
Thanks,
Masumi
Hello Masumi,
It looks like that the device does come in two types of Pin-1 marking and they are both correct. The convention for most plastic rectangular packages is to look at the package in the horizontal direction and read the text/marking on it correctly from left to right. Pin 1 is then in the lower left corner. In the A-Type image, Pin 1 is also indicated with the help of the Dot. In the B-type image the horizontal bar on the package helps identify the edge of the package on which Pin 1 is located. The remaining pins are numbered counter-clockwise across the bottom and around to the top. Hope this was of help, let us know if you have more questions. Thanks!
Regards,
Srikanth