hello
I have a question about how to stop charging and discharge the battery.
When an adapter is connected (VBUS supply = 5V to 20V) Is there any way to stop charging and switch to battery operation Is there a way to stop charging and switch to battery operation?
This is for battery capacity calibration.
I would like to force the device to switch to battery operation and discharge the battery with the circuit load, and then recharge the battery when the battery capacity drops below a certain threshold.
I have checked the LEARN function, but I am not sure if this function can be used.
The LEARN function switches to adapter operation when the battery voltage drops below a certain level, so I don't think I can achieve my desired operation.
Thanks in advance.