This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3.3V to -3.3V with 1.5A output current solution

Other Parts Discussed in Thread: TPS566238, TPS82130, TPS62903

Hi team

Could you help give a solution for this application?

  • Vin=3.3V
  • Vout=-3.3V
  • Iout=1.5A
  • Small-size solution

I first think of two devices: TPSM82130 and TPS566238, but

  • TPSM82130 output current is less than 1A under 3.3V to -3.3V condition.
  • TPS566238 fsw is only 600kHz, which cause a large total solution size.

Could you help give you comments on this opportunity? Thank you.