Other Parts Discussed in Thread: BQ24610
I made a stand alone Li Charger board using the BQ24618, following the schematic in the datasheet. We built them and it does not run. It seems to try for 16ms, then stops for 28ms and repeats. I see a pulse on the LODRV that causes a ripple on PH and BTST just before the chip seems to reset. I tried 2 boards and they did the same thing. I could just start replacing parts one by one to see if Production used a wrong part. I was hoping if someone could point out a mistake or direct me to a particular area that I should focus on. I would think that BTST would go high to 10V or so, but it stays down around VBAT/PH.
Thanks