This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4040-N-Q1: Negative reference generation

Part Number: LM4040-N-Q1
Other Parts Discussed in Thread: LM4040

Hi,

I want to generate negative -2.5V using LM4040AIM3-2.5/NOPB reference IC.

I have one LTSPICE simulation model for LM4040 which gives 3V reference output. I tried connecting -15V to anode as shown below and the model is not working.

Can we generate a negative referencing by giving negative supply at anode of Zener reference IC LM4040?

Can you please provide SPICE model for  LM4040 for any of the reference voltage.

Thanks,

Namita