Hi team,
What is the PSRR level for this device when operated at 5V 3A output?
Thanks!
Lauren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
What is the PSRR level for this device when operated at 5V 3A output?
Thanks!
Lauren
Hi Lauren,
Figure 21 has PSRR data for VOUT = 3.3V, IOUT = 3A. This plot can likely be used to approximate the PSRR for the given specifications because the important operating conditions are specified in the plot - namely VIN, VOUT, IOUT. The trend for PSRR is that with constant load, increasing the VIN - VOUT differential increases PSRR. More generally, moving farther away from dropout increases PSRR. So, if the input voltage in this application is larger than 5.5V, the PSRR will be better than the VIN = 3.8V, IOUT = 3V curve in this plot. Attached is a slideshow discussing the things that do and do not effect PSRR for reference.
Regards,
Nick