Hi all,
I have problem with my BQ34Z100-G1. After performing a successfull learning cycle, and running some satisfying tests, I have encountered a problem.
I have tried a particular charging/discharging profile which is close to my application. In it, there are sudden changes between charge and discharge so the current can quickly go from 6 A to -6A for instance (with 12 V lead acid agm 90 Ah battery), and it seems that when that happens, the TRUE FCC suddenly changes by a large value, completely false.
Then after some time, FCC gets to TRUE FCC and my SoC gauge becomes totally wrong (not the good SoC calculated).
Enclosed is a log file of 5 days of testing.
At some points in time, it is possible to see those sudden changes, for instance:
22-10-2021 at 17:03:30
26-10-2021 at 01:49:13
25-10-2021 at 23:29:16
and many other times.
This is TRUE FCC which suddenly changes, sometimes by a very large value (18 965 mAh to 10 335 mAh for instance for 25-10-2021 at 23:29:16). This is obviously completely wrong as my capacity can not decrease that much. Also after a while (too late), or after a complete charge, the TRUE FCC comes back to around its normal value (around 18 500 mAh).
I would like to know how we can prevent this problem from happening as this makes my SoC gauge completely useless and wrong.
Thanks a lot in advance for your help.
Regards
Lucas registre.log