Hi team,
My customer's supply seems to be current limiting on a board with TPS63900. The input current seems to be around 80 mA when the convertor appears to brown-out.
If they have Rcfg1 set to 36.5Kohms, Rcfg2 set to 0 ohms, Rcfg3 is set to 0 ohms. This gives Vout = 3.3V
Sel = High
So shouldn’t they be getting unlimited current limiting on the input?
For the output it should be typical 1.45 A peak switching current limit. Is this correct? (1.33 to 1.6 A)
Thanks,
Connie