Hello,
We are facing with accuracy of current measurement and coulomb counting at low currents (10-50mA). We have used 3 sense resistor in parallel (1mohm each)as seen below. The voltage when measured across these sense resistors at low currents in not as expected. The current of 10-50mA is flowing through R_NT1. No current is flowing from PACK- to BAT-.
When an accumulation of 100mAh is expected at 10mA load after 10hrs, we are getting only 30mAh. We are expecting issue with sense resistor layout (Kelvin connection design) or position of Net Tie (R_NT1). Please suggest what you think.