This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: LM5022 in SEPIC, IC fails, runs hot

Part Number: LM5022

I have an LM5022 in SEPIC configuration, that I can vary from 5-35VDC. Maximum continuous current is about 1.5A, and pulsed current is as high as 5A for short durations. The output is connected to an LED current source circuit to drive power LEDs.

Problem I have is that occasionally (about 1 out of every 10 or so) assemblies, the LM5022 appears to fail immediately (upon power up, or when the load is first connected). The LM5022 body will become very hot and draw large amounts of current. Replacing it generally will fix the issue.

I am not sure what could be causing this intermittent issue and I have not been able to replicate when or how this fault occurs.