This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22912C: Current consumption of enable-pin

Part Number: TPS22912C


Hi, 

I would like to drive TPS22912's with microcontroller, but want to know the current consumption of its ON-pin.

If just look at the VOH, VOL of microcontroller and VIH, VIL of the load switch, I need a level converter IC in between.

Meanwhile, microcontroller's VOH's and VOL's voltage margin, basically depends on the sinked current of the ON-pin of load-switch,

which means the lower the current, the lower the VOH's  and VOL's voltage drop. If the sinked-current of ON-pin is just a micro order of Ampere, I think I don't need level-converter IC, but if it is around 1-3mA, 

I need it.

Thanks