This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51215A: Equation for inductor and ripple current on datasheet

Guru 19645 points
Part Number: TPS51215A

Datasheet P16 is described about inductor and ripple current.

Example case is described 25%, but equation is using "×0.4". 

If there any reason or background for above difference, please let me know.

Best regards,

Satoshi

  • Hi Satoshi,

    I do believe the datasheet contains a typo in the example outlined on page 16. In this example, 0.4*30=12A for the inductor ripple current, so the inductor value is calculated assuming the inductor ripple current is actually 40% of the full load output current. In our designs, we typically recommend the inductor ripple current be between 10% and 40% of the output current level for a balanced design (in the case of this part the 25%-50% recommendation is also acceptable).

    I apologize for any confusion, and I will work with the appropriate product owners to address this fix.

    Regards,

    Alec Biesterfeld