This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does TI have a P2P solution like to Si8273BB-IS1?

Other Parts Discussed in Thread: UCC21520, UCC21521, UCC21530, UCC21222, UCC21540

Hi team,

Does TI have a P2P solution like Si8273BB-IS1?  spec must be same or upgraded. thx 

  • Hi Jimmy,

    Thank you for reaching out to E2E!

    Please allow us until tomorrow to get back to you for this cross. Our experts are looking into the proper device that we can position here.

    Thank you for your patience.

    Best regards,

    Andy Robles

  • Hi Jimmy,

    Our most compatible P2P solutions for the Si8273BB are:

    • UCC21520 - Almost P2P, it has disable pin instead of Enable. It has programmable dead time control. The package is wider, supports higher isolation voltage 5.7kVrms.
    • UCC21521 - Is P2P but without the Q100 qualification. It has a wider package.
    • UCC21530 - Greater channel to channel spacing because 2 pins are removed. Is P2P, has enable pin and dead time. The package is wider, supports higher isolation voltage 5.7kVrms.
    • UCC21222 or UCC21220- Almost P2P, has disable pin. These are the only dual channel drivers in a 16-NB package.
    • UCC21540 - Almost P2P, similar to the UCC21520 and UCC21530, more flexibility and has disable pin only. 

    Regards,

    Krystian

  • Hi team,

    thanks for your great support, maybe will consider using UCC21521 to design. thanks