This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92690: LOW duty PWM doesn't work

Part Number: TPS92690

Hello Sir,

if apply PWM 200Hz 0.5% duty to PIN1 nDIM, the backlight turns on after 22seconds, 

if apply PWM 200Hz grater than 10% to PIN1 nDIM, the backlight turns on in 3 seconds,

is any suggestion of it.

the attached picture shows PMW and ouput voltage,

10 LEDs in serial, 6 in Parellel, current 242mA, LED voltage 56V.

the yellow curve is 200Hz 0.5% PWM,

the green curev is LEDvoltage.

thanks!

Wiht best regards,

PZ