Other Parts Discussed in Thread: TPS61169
Hello TI support,
I have been researching multiple backlight LED drivers for controlling a string of LEDS. For example 6 LEDS per channel. I need the LEDs to be turned on at a steady current for 2 seconds, turned off for about 7 seconds and then repeat forever. We are backlighting a series of semitransparent objects that are passing by a global shutter camera. Using the exposure control of the camera to (somewhere between 10 and 40usec/image) capture images of the objects as they move past the camera. Expect drive current range is 20 to 40 mA. The part numbers for the LEDS are: "LB P4SG", "ATS2012UV415". We can't use a PWM or pulsed output because it will reduce resolution in each image captured. Therefore, I want to use the pure analog control for controlling the brightness of the LEDs. Since I will be driving the LEDs in a range from 20mA to 40mA, I would think that pure analog control will work since I am driving greater than 25% of the LED current. Please let me know what your thoughts are and if this product will work or if there are any other parts that might be better for my application. I have four LED drivers that I picked out, this one in this support ticket has all three dimming options, PWM control, analog control, and hybrid PWM dimming. In addition, please let me know if there is anymore information that I need to provide to you.