This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Is a UCD90xxx PMBus command reference required?

Expert 4165 points

Not necessarily, and it is up to what you plan to do. However, do use it as an ultimate reference. Each function in the Fusion GUI has a corresponding PMBus command. The UCD90xxx PMBus Command Reference contains not only protocol information but also a description of the device behavior of each function. If a customized software driver is required to develop to communicate with the UCD90xxx device, this UCD90xxx PMBus Command Reference is necessary.

UCD90xxx PMBus Command Reference 

For more FAQ please check the following document.

UCD90xxx Family Frequently Asked Questions and Answers