No. A data flash image file can only be generated from a live device or a data flash script file. When offline, the GUI can generate a project file (.xml), which can be imported to the live device to generate a .hex file and PMBus write script file.
For more FAQ please check the following document.
UCD90xxx Family Frequently Asked Questions and Answers
UCD9090 UCD9090A UCD90120 UCD90120A UCD90124 UCD90124A UCD90160 UCD90160A UCD90240 UCD90320 UCD90320U