This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPSM846C24: How to calculate the FIT rate for this module?

Part Number: TPSM846C24


For modules, the FIT is calculated differently.

This is a  module assembly made of up individual components (unlike solid state silicon). As such this reliability prediction is based on TR-NWT-332 Reliability prediction model that uses a parts count methodology rather than Burn-in data used for silicon. The inherent reliability of each component is based on data in the  TR332 model and then factored assuming a 50% electrical stress of rated maximum and also as at 40C operating environment. The failure rate of each component is then summed  to give the failure rate of the module.

 The way to calculate FIT rate for modules is to use the MTBF given in the datasheet.

FIT = (1/MTBF)*10^9 = 1/26600000 * 10^9 = 37.59

 FIT = 37.6