Other Parts Discussed in Thread: LMR16006
Hello,
I have build a circuit of 4 channel led driver using 4 tps54201 parts. The board is very small 1.5cmx3cm. i have packed all parts same way and close each other. The inductors are unshielded. The current is set to 200mA. On the bottom side i have small uC located for dimming control. All parts are supplied from the same source, 15V.
Always, one of the tps54201 is dieying after a few seconds. There is no shortcircuit on the board. Is there any chance that one TPS interfere to others?