Other Parts Discussed in Thread: GPCCHEM, , BQ4050
Dear Expert
As for the questions I told you over the phone, please help me confirm them:
1. The minimum current of full charge is 80 seconds, can it be shortened?Could it be 20 seconds or 10 seconds?
2. Is continuous discharge required during cyclic learning?Does charging for a short time during discharge affect cyclic learning?
3. Will the SOC deviation of coulometer jump from 2% to 8% or 100% after the factory cycle learning and shipment?Does the user need to repeat the loop learning process?