This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1020: Maximum current

Part Number: LMG1020
Other Parts Discussed in Thread: ALLIGATOR

Hi Team, assisting a client.

They would like to use the LMG1020 device for switching a GaN device GS66508B at 27.095 MHz (So there is a periodic signal not just one pulse). In the preliminary design, they used 22 Ohm resistors between OUTH, and OUTL (connected in parallel) and the GaN input at the gate.

It seems that these resistances are giving very long charge (OUTL)/discharge (OUTH) time, so at 27.095 MHz the OUTL voltage varies between 0 and 2v, and OUTH varies between 3.6 and 5 v. As a result, the GaN just experiences a slight change in the Q point position and not a complete on/off cycle as it should do.

They are considering to minimize these resistors. However, they am puzzled as to what combination of values could work best for their case. In the LMG1020YFFT data sheet, the OUTL series resistor is "optional". Various references give various values for the values for these resistors, and the series resistors are zero in the evaluation board used here. This could results in significant shortening of time lag if the maximum current values quoted in the LMG102 datasheet are respected.

Hoping for your input.

Thank you.

-Mark