This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4101: 6pin and 7pin be shorted to the VIN

Part Number: TPS7A4101


Hi team,

Can the TPS7A4101 6pin and 7pin be shorted to the VIN?
The reason for asking this question is that my customer used the TPS79801 in old projects and shorted 6pin and 7pin to the VIN(as Figure1), and now they want to P2P replace the TPS79801 with the TPS7A4101 and do not change the original design (due to supply issues). So I want to ask if the TPS7A4101 can be connected like this?
If the TPS7A4101's 6pin and 7pin are shorted to the VIN, there exist any risk? 
Could you please help give some comments? Thank you!
 

Figure 1

Regards,

Ivy