This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548D22: Tolerances

Part Number: TPS548D22

The datasheet only specifies line and load regulation as well as output voltage ripple at a specific example.

Would it be possible to have access to the general end of life tolerances of line regulation, load regulation and output voltage ripple.

Best Regards,

Greg A

  • Hi Greg,

    Our US team will check this and reply you soon.

  • Hi Greg,

    I do not have any specific data related to load and line regulation at the end of the product's life. The data in the datasheet regarding load and line regulation generally hold over the life the product.

    As you mentioned the load and line regulation in the datasheet are specified in the design example, but I would say that the 0.5% spec for both load and line regulation is valid especially if the output voltage matches the reference voltage (ie RSP and RSN are tied directly to the output without the need to factor in feedback resistor tolerance). 

    Regards,

    Alec Biesterfeld