Hi,
I am using TPS652353 in my design and using I2C to control it.
It works fine for setting voltage levels, I am using 13.4V and 18.2V which work fine.
But. when I try to disable the output by writing 0x00 in Control 2 register, the voltage output comes to 14.6V instead of 0V.
What can be the issue?
This is what I am writing via I2C to switch off the LNB output
Wire.beginTransmission(0x09); //address of the device
Wire.write(0x01); //control2 register address
Wire.write(0x00); //data byte
Wire.endTransmission();