This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61176: Output missing.

Guru 10775 points
Part Number: TPS61176

Hi team,

In mode4, if a 120Hz PWM signal is an input, the output will be lost sometimes.
Blue : IFBx
Green : Input PWM signal


This phenomenon only occurs in mode4.
It also occurs when Duty is 10% to 0.5%.
It does not occur below 0.5%.
Could you tell me why happen this?

Sincerely.
Kengo.