BqStudio launches for gas gauges to the Registers tab. Menus and tables for Registers, Bit Registers, Commands and Log panels are displayed. It is possible to move these windows and adjust their sizes so that all of the registers, bit registers and commands are displayed without have to scroll. But when I do this and close and re-open bqStudio, these changes are not retained.
How do I get these changes to be retained, and how can I default the Auto Refresh feature to off when I reopen bqStudio?