Hi
I was using UCC21520 in one of our application(Inverter). DC bus voltage is 48Vdc. Secondary of High Side drivers are supplied by each isolated flyback converter and all three low side drivers are powered with single flyback converter. output of flyback converter is +15V and -8V. With inductive load suddenly the driver output is not same as input. as show in below image for top. Driver output for top going low for some duration even when primary of input is high.

I have change the Rgon from 10ohm to 5.6ohm and Rgoff from 5.6ohm to 2.2ohm. still the problem remains same. During testing i also monitored the supply voltage levels at totem pole transistor(booster) Q5 and Q6 collector as below image . They are stable and no issue found. Also checked DT pin and Disable pin status they are also healthy.

I would like to know what could be the reason for driver blocking the pulse.
Regards
Bharath Gilla