This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS768: abs. max and recommended Tj and Ta of TPS768 and TPS768-Q1

Part Number: TPS768

Hi team,

I have a question about the abs. max and recommended Tj and Ta of TPS768 and TPS768-Q1.

In the datasheet of TPS768, I can see the abs. max Tj = -40 to 125C, recommended Tj = -40 to 125C.

In the datasheet of TPS768-Q1, I can see the abs. max Tj = -40 to 150C, recommended Ta = -40 to 125C.

Additionally, the datasheet of TPS768 (above) and TPS768-Q1 (middle and bottom) say the same thing.

So I am confusing now.

  

1. Why are the abs max Tj and recommended Tj same on TPS768?

2. What are the Abs max Tj and Ta and Recommended Tj and Ta for each TPS768 and TPS768-Q1?

  Are there any differences?

best regards,

Yuto