Hi,
Customer have used LM5015 for a 48V input ,5V2A output flyback design as below. it works fine. they would like to make a small change to support input 12V for another product, but still can support 5V2A. .
if nothing change with 12V input, the output is only 3.5V. then they tried to double the coil turns at secondary side, the output is 5V, but load capacity is very weak, the output drop to 4.7V with 600mA. this device is kind
old, WEBENCH doesn't support. could you please suggest how to make a small modificaiton to support this case? thanks.