This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24170: Change Using 12V to 5V,USB

Resolve

  • Hello,

    What is your battery voltage when this is happening? The input voltage must be above the battery voltage because this is a buck charger.

    Also, you will need to adjust your OVPSET divider. With a 5 V input, OVPSET is 0.45 V which is below 0.5 V and indicates undervoltage.

    Thanks,

    Mike Emanuel

    Please click "Resolved" if this answered your question.