Other Parts Discussed in Thread: GPCCEDV, BQSTUDIO, ,
Hi team,
The customer would like to figure out the following questions:
1.The parameters EMF, EDVC0, EDVC1, EDVR1, EDVR0, EDVT0 are obtained after the low and high temperature light load. Max error is still 100% when the EDDTC is populated in BQstdio, why is that?
And what additional parameters are required to implement the Max error change?
2. The capacity of the charged and discharged battery is still not accurate after the high and low temperature light load of the CEDV battery. Are there any specific steps to get the capacity correctly?
3. The following are the CEDV parameters for the output, several of them VOC75, VOC50, VOC25, and the OCV corresponding to the SOC, the customer cannot dose not know where to put them in BQstdio.
Do the following parameters need to be populated in BQstdio?
Could you help resolve this case? Thanks.
Best Regards,
Cherry