Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22679: LM22679-5p0_AVG for loop stability test

Part Number: LM22679

Hello, 

I completed my design with LM22679-5p0_TRANS model, and now I would like to test loop stability. My understanding is that I should replace TRANS model with the TM22679-5p0_AVG model, and properly connect VIN, FB, SW and GND pins. The remainder of my circuit should remain the same. I am using LTSpice, so I am following steps in this document. Is there anything wrong in the steps I am taking? 

One additional question I have: Do I need to change any parameters in the AVG model? For example, there is parameter L=6.8u. If this is an inductor value, do I need to change this to match my inductor? 

Thanks!