Hello, I am working on a design similar to the reference one, but with 24V 25A output.
I had Vbias ON in the control circuit and looking on an oscilloscope at the rectangular signals from the FET gates. After that, when I connected the 400 VDC input to the power circuit, the circuit lines and FETs (Q2 and Q3) blew up.
Do you know why this can happen?

Before the explosion, I tried a larger R value on the gate control primary (R33 and R34) with a lower control current. In this test I got a 24V 300mA output, but the H-bridge control FETs got really hot and I quickly shut down. I understand that the current and voltage control gate was not sufficient to drive the FETs. Finally I put 3ohm into R33 and R34 as the original circuit when it blew up.
Thanks
Ezequiel