Part Number: BQ25792
We're trying to implement some form of power down on our device using the Ship FET on the BQ25792. /QON is connected to a momentary switch to ground and one of our controller GPIOs. The idea was to have the controller detect a short button press then place the charger in ship mode over I2C then have the charger wake up using the same switch on /QON. When we implemented this I could see that the controller was detecting the button press correctly and got the message that it was writing to the charger to select Ship Mode. At this point I expected to see the power supplies fed from the Sys Out of the charger to shut down taking the controller with them. Nothing happened. As a sanity check, I held the button for 20s verifying that the /QON pin on the chip was low expecting to see a reset. Again, nothing happened. I monitored the SDRV out and didn't see any activity when I tried the system reset. Any other suggestions for debugging this issue? Out ship FET is an infineon BSC120N03LSGATMA1 with a Vgs(th) similar to the TI FET on the EVM board.