Hi,
I am trying to use TPS55288 for Power delivery 5V/9V/15V/20V, i set current limitation is 5A.
But when over 2.5A loading in all voltage setting, its output voltage was drop down.
I suppose some protection was occurred.
I2C setting is below, and circuit diagram is attached.
Please advice what i should change for 5A current.
[I2C setting in case 20V output]
| Register Address | Register Name | 20V output | Meaning |
| 0h | VREF [7:0] | 0xC0 | 1129mV |
| 1h | VREF [9:8] | 0x03 | |
| 2h | Current Limit | 0xE4 | 50mV/10mΩ = 5A |
| 3h | Slew Rate | 0x01 | Default |
| 4h | Feedback Selection | 0x03 | Internal FB, FB ratio to 0.0564 |
| 5h | Cable Compensation | 0xE0 | Default |
| 6h | Mode | 0xA4 | Output enable, 0x75h, |
[Circuit Diagram]

Regards,
Hirosawa