HI
The data sheet says that when the cs pin of the lm5022 becomes 0.5V, it does not work.
So I shorted it to allow overcurrent to flow.
However, the voltage on the cs pin does not rise to 0.5V and the operation does not stop.
Can you tell me why??
*INPUT : 14.1V~32V OUTPUT : 12V 1A