This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A92: Performance comparison between TPS7A92 and LP38798 for PLL user case

Part Number: TPS7A92
Other Parts Discussed in Thread: LP38798

Hi team,

We used to use LP38798 to power PLL device in radio system. And now we want to use TPS7A92 to replace it. How could i judge which device performance is better? From noise density aspect, both device is ~5uVrms, but the PSRR performance have a large difference. 

The user case is that: 

Vin:3.68V, Vout=3.3V, Io=600mA. Vin is coming from DCDC, which fs=700kHz~1MHz. 

Thanks in advance

 B.R.

Lucas