Hello Expert,
Our customer have questions for BQ24253.
I confirmed datasheet and it said that EN0/1 setting is applied if there is status change after D+/D- detection.
Our customer plan to configure each pin just connecting GND or power supply rail for achieving 900mA ILIM for using USB3.0 application.
Does it mean that EN0/1 setting doesn't applied if they use D+/D- detection?(except DCP)
As far as my understanding D+/D- detection cannot define Vin_DPM.
However, this pin setting depend on EN0/1 status and truth table seems EN0/1 haven't applied if EN0/1 status don't have any change.
When, what does Vin_DPM setting applied during the timing of D+/D- detection completed?
Also, I found explanation that this device can support USB3.0 on datasheet p21 but there isn't detailed explanation.
Then, would you tell me suggested setting supporting USB3.0?
By the way, I'd like to change CBOOT from from 33nF to 47nF.
Is this modification acceptable?
Sorry for rushing you but I want to get answer for these questions by tomorrow.
I'm waiting your answer.
Best regards,
Kazuki Kuramochi