Hello,
My customer plans to design a power supply block using TI's devices as shown below.

The customer has some questions about the operation of the BQ2459.
1. If they used a 317ohm resistor on the ILIM pin of the BQ24259 to limit the current to 1.5A, would the total supply wattage be 7.5W?
2. Is it possible to output the rest of the power source except for the battery charging in the BQ24259 as a bypass?
3. Is it possible to send all input power to the output when no battery is connected to the bQ24259?
4. Can the customer turn the BQ24259 output on/off while charging the battery?
Thank you.
JH