This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS2660: Shutdown pin and AVDD details

Guru** 105791 points
Part Number: TPS2660

Can you share internal structure details of SHDN/ pin ?

  • SHDNb pin has internal pullup as shown in the below equivalent circuit. So, it can be left OPEN if you wish not to control the device remotely.

    The typical voltage of AVDD is 4.275V. The internal clamp sets the open-circuit voltage of 2.7V (typ) at the SHDNb pin