Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hi,
We would like use BQ34Z110 to get our batterie gauge (only). Our batteries are 12S NiMH.
We have install BQstudio/EV2400 and get values from the IC. The values returned are close to be good.
In scan mode, the Register page has activity depending on current direction.
The button PIN_CONTROL_EN change the PCTL_EN (bit4-Manufacturer status)
But we can't modify any value:
- We tried the Calibration but it has no changes on the values (I/V/T) measured
- If we change the number of serial cells (default =1) to 12 / press Write_All / press Read_All, the value is reset to 1.
- same for design_capacity_mAh of data_memory, impossible to fix.
- Sec1 & Sec0 in full access (already checked)
Can you help me to pass this point where nothing seems use-able. The IC is running but we can't do anything !
Thanks
our BQstudio view :