Other Parts Discussed in Thread: UCC27212
Hi,
I got a UCC27212EVM-328 the other day.
I have changed Nch-FET with IPD5N25S3
and 4.7nF/50V/X7R and 1nF/50V/X7R in parallel on the Cboot.
because I have to operate at 3MHz frequency. This is lower Qg, Ciss, Rise time, Fall time than before.

So, I'm testing it. but UCC27212 IC is so hot. temperature is about 85 °C
VDD 12V, 0.08A
HV 12V, 0.3A
The picture below is HIN , LIN signal and HO, LO signal in UCC27212 IC.


I want to know why UCC27212 IC overheat.
is it possible UCC27212 IC to operate at 3MHz, High Voltage?