Hi team,
Could you advise how does the device behaves in the conditions below?
This is the automotive application.
BATT=9V to 16V
| IN | GND | 出力 | |
| 1 | BATT | GND | BATT |
| 2 | BATT | GND | GND |
| 3 | Open | GND | BATT |
| 4 | Open | GND | GND |
| 5 | BATT | Open | BATT |
| 6 | BATT | Open | GND |
Please correct if my idea below is wrong.
1. Protected. Device keeps operation.
2. Protected. Trigger current limit and eventually trigger thermal shutdown and repeat it. (not good for reliability)
3.Current flow through body diode and charge input capacitor to power up the device.
VIN<Vout - 1x diode which violate the absolute maximum ratings, but the current is limited(VIN=open). So risk is low?
4. Protected. No problem.
5. Protected, No problem.
6. Protected. Trigger current limit and eventually trigger thermal shutdown and repeat it. (not good for reliability)
regards,