Other Parts Discussed in Thread: TPS62867, , TPSM82810
Is the output discharge resistor capable of discharging very large output capacitances without concern of damage?
For instance, we have a case where 1000uF will be connected on the output at 1.8V and an expected die temperature of 110C.
I see that the discharge resistance is typically ~ 3.5 ohms but more like 4.5 ohms when the die is hot (assuming 5V input)
For infinite capacitance (essentially a constant 1.8V on the output with the device forced off), I'd expect to see (1.8V^2)/4.5ohms = 720mW dissipation in the discharge resistorand a temperature rise of 25.4C/W * 0.72W = 18.3C. I think the 1000uF discharge would be ok ( ~ 4.5msec RC) but it's not clear due to the various thermal time constants.
Will the device be ok for the 1000uF, 1.8V scenario described? Is there an energy rating on the discharge resistor?

Best Regards!
Steve