This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS2662: Can I connect RTN to GND ?

Guru** 105361 points
Part Number: TPS2662

Can I connect RTN to GND ?

  • Yes... In designs that do not need reverse input polarity protection can have RTN, GND and PowerPAD connected together. In these designs, PowerPAD of the eFuse can be connected to the PCB ground plane for an enhanced thermal performance.

    NOTE: If your system needs Reverse Polarity protection feature, "Do not connect RTN to GND"