Other Parts Discussed in Thread: TLC6983, , TLC6946, TLC6948
Hello,
we are looking for RGB LED matrix solution (64x16 RGB LEDs) to drive a led panel asynchronous to the data bus.
I found the TLC6983 but unfortunately this is common cathode and most LEDs on the market are common anode.
So now I found the TLC5958, but I am confused if it is possible to use it asynchronous. The Data line is only about 100 kb/s to update the SRAM.
But the display framerate should be at least 200 Hz.
I would like to ask for the Application Note: “Build High Density, High Refresh Rate, Multiplexing LED Panel with TLC5958.”
Or can you recommend another device for that purpose?
Best regards